CameraBuilderStockLens Enumeration¶
NXOpen.Display.CameraBuilder.StockLens is an alias for NXOpen.Display.CameraBuilderStockLens
-
class
NXOpen.Display.
CameraBuilderStockLens
¶ Bases:
object
Predefined lenses: 28, 35, 50, 70, 105, 135, 210, 300mm
Enum Members
Enum Member Enum Member Description S28 28mmS35 35mmS50 50mmS70 70mmS105 105mmS135 135mmS210 210mmS300 300mm-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-