CameraBuilderLensFlare Enumeration¶
NXOpen.Display.CameraBuilder.LensFlare is an alias for NXOpen.Display.CameraBuilderLensFlare
-
class
NXOpen.Display.
CameraBuilderLensFlare
¶ Bases:
object
Predefined lens flare types: Standard, 35mm, 50mm, 105mm, polygonal, 35mm poly, 50mm poly, 105mm poly, spark, star
Enum Members
Enum Member Enum Member Description Standard Standard lensS35 35mmS50 50mmS105 105mmPolygonal polygonalP35 35mm polyP50 50mm polyP105 105mm polySpark spark lensStar star lens-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-