BoundedGridBuilderLabelReferenceType Enumeration¶
NXOpen.Display.BoundedGridBuilder.LabelReferenceType is an alias for NXOpen.Display.BoundedGridBuilderLabelReferenceType
-
class
NXOpen.Display.
BoundedGridBuilderLabelReferenceType
¶ Bases:
object
Specifies label reference.
Enum Members
to determine grid line offset labels “
“Wcs”, ” Use projection of WCS origin on thegrid plane to determine grid line offset labels “
“Absolute”, ” Use projection of absolute origin on thegrid plane to determine grid line offset labels “
-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-