BackgroundType Enumeration¶
NXOpen.Display.Background.Type is an alias for NXOpen.Display.BackgroundType
-
class
NXOpen.Display.
BackgroundType
¶ Bases:
object
background types
Enum Members
Enum Member Enum Member Description Plain single color backgroundGraduated two color background, which varies between themImage an image file displayed in the backgroundHemiDome an 3D HDR image displayed in the background-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-