WearPlateLocChildBuilderPositionType Enumeration

NXOpen.Die.WearPlateLocChildBuilder.PositionType is an alias for NXOpen.Die.WearPlateLocChildBuilderPositionType

class NXOpen.Die.WearPlateLocChildBuilderPositionType

Bases: object

Settings for the positioning of the locator relative to the wear plate.

Enum Members

Enum Member Enum Member Description
Left
Position locator to the left of the wear plate.
Right
Position locator to the right of the wear plate.
Both
Position locator on both sides of the wear plate.
Neither
No locators.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.