TrimFlangeDieAssistantBuilder Class¶
-
class
NXOpen.Die.
TrimFlangeDieAssistantBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a
NXOpen.Die.TrimFlangeDieAssistantBuilder
To create a new instance of this class, use
NXOpen.Die.DieCollection.TrimFlangeDieAssistant()
New in version NX5.0.0.
Properties¶
Property | Description |
---|---|
Clearance | Returns or sets the clearance used in the automatic generation of the lower post flange profile |
FlangeProfile | Returns the flange profile |
FlangeProfileSet | Returns the flange profile set |
LowerBase | Returns or sets the lower base |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
PierceLocations | Returns the pierce locations |
SheetMetal | Returns the sheet metal |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Thickness | Returns or sets the thickness |
TrimProfileSet | Returns the trim profile set |
UpperBase | Returns or sets the upper base |
Methods¶
Method | Description |
---|---|
AutoGen | TODO: fill in a description for this |
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
FlangeSteelRestrikeParms | TODO: fill in a description for this |
FlangeSteelWipeParms | TODO: fill in a description for this |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
LowerPostParms | TODO: fill in a description for this |
LowerScrapCutterBaseParms | TODO: fill in a description for this |
LowerScrapCutterParms | TODO: fill in a description for this |
NewFlangeProfile | Creates a new flange profile item in the set @return |
NewTrimProfile | Creates a new trim profile item in the set @return |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
TrimSteelParms | TODO: fill in a description for this |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
UpperPadParms | TODO: fill in a description for this |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Clearance¶
-
TrimFlangeDieAssistantBuilder.
Clearance
¶ Returns or sets the clearance used in the automatic generation of the lower post flange profile
-------------------------------------
Getter Method
Signature
Clearance()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Clearance(clearance)
Parameters: clearance (float) – New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
FlangeProfile¶
-
TrimFlangeDieAssistantBuilder.
FlangeProfile
¶ Returns the flange profile
-------------------------------------
Getter Method
Signature
FlangeProfile()
Returns: Return type: NXOpen.ScCollector
New in version NX5.0.0.
License requirements: None.
FlangeProfileSet¶
-
TrimFlangeDieAssistantBuilder.
FlangeProfileSet
¶ Returns the flange profile set
-------------------------------------
Getter Method
Signature
FlangeProfileSet()
Returns: Return type: NXOpen.Die.DieAssistantFlangeProfileList
New in version NX5.0.0.
License requirements: None.
LowerBase¶
-
TrimFlangeDieAssistantBuilder.
LowerBase
¶ Returns or sets the lower base
-------------------------------------
Getter Method
Signature
LowerBase()
Returns: Return type: NXOpen.Plane
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
LowerBase(lowerBase)
Parameters: lowerBase ( NXOpen.Plane
) –New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
PierceLocations¶
-
TrimFlangeDieAssistantBuilder.
PierceLocations
¶ Returns the pierce locations
-------------------------------------
Getter Method
Signature
PierceLocations()
Returns: Return type: NXOpen.SelectPointList
New in version NX5.0.0.
License requirements: None.
SheetMetal¶
-
TrimFlangeDieAssistantBuilder.
SheetMetal
¶ Returns the sheet metal
-------------------------------------
Getter Method
Signature
SheetMetal()
Returns: Return type: NXOpen.SelectBody
New in version NX5.0.0.
License requirements: None.
Thickness¶
-
TrimFlangeDieAssistantBuilder.
Thickness
¶ Returns or sets the thickness
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: float New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Thickness(thickness)
Parameters: thickness (float) – New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
TrimProfileSet¶
-
TrimFlangeDieAssistantBuilder.
TrimProfileSet
¶ Returns the trim profile set
-------------------------------------
Getter Method
Signature
TrimProfileSet()
Returns: Return type: NXOpen.Die.DieAssistantTrimProfileList
New in version NX5.0.0.
License requirements: None.
UpperBase¶
-
TrimFlangeDieAssistantBuilder.
UpperBase
¶ Returns or sets the upper base
-------------------------------------
Getter Method
Signature
UpperBase()
Returns: Return type: NXOpen.Plane
New in version NX5.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
UpperBase(upperBase)
Parameters: upperBase ( NXOpen.Plane
) –New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
AutoGen¶
-
TrimFlangeDieAssistantBuilder.
AutoGen
¶ TODO: fill in a description for this
Signature
AutoGen()
New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
FlangeSteelRestrikeParms¶
-
TrimFlangeDieAssistantBuilder.
FlangeSteelRestrikeParms
¶ TODO: fill in a description for this
Signature
FlangeSteelRestrikeParms()
New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
FlangeSteelWipeParms¶
-
TrimFlangeDieAssistantBuilder.
FlangeSteelWipeParms
¶ TODO: fill in a description for this
Signature
FlangeSteelWipeParms()
New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
LowerPostParms¶
-
TrimFlangeDieAssistantBuilder.
LowerPostParms
¶ TODO: fill in a description for this
Signature
LowerPostParms()
New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
LowerScrapCutterBaseParms¶
-
TrimFlangeDieAssistantBuilder.
LowerScrapCutterBaseParms
¶ TODO: fill in a description for this
Signature
LowerScrapCutterBaseParms()
New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
LowerScrapCutterParms¶
-
TrimFlangeDieAssistantBuilder.
LowerScrapCutterParms
¶ TODO: fill in a description for this
Signature
LowerScrapCutterParms()
New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
NewFlangeProfile¶
-
TrimFlangeDieAssistantBuilder.
NewFlangeProfile
¶ Creates a new flange profile item in the set
Signature
NewFlangeProfile()
Returns: Return type: NXOpen.Die.DieAssistantFlangeProfile
New in version NX5.0.0.
License requirements: None.
NewTrimProfile¶
-
TrimFlangeDieAssistantBuilder.
NewTrimProfile
¶ Creates a new trim profile item in the set
Signature
NewTrimProfile()
Returns: Return type: NXOpen.Die.DieAssistantTrimProfile
New in version NX5.0.0.
License requirements: None.
TrimSteelParms¶
-
TrimFlangeDieAssistantBuilder.
TrimSteelParms
¶ TODO: fill in a description for this
Signature
TrimSteelParms()
New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
UpperPadParms¶
-
TrimFlangeDieAssistantBuilder.
UpperPadParms
¶ TODO: fill in a description for this
Signature
UpperPadParms()
New in version NX5.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
TrimFlangeDieAssistantBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.