Tip Class¶
-
class
NXOpen.Die.
Tip
¶ Bases:
NXOpen.Features.Feature
Represents a Tip feature.
This class supports operations on a Tip feature, see TipBuilder for creation.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AlgorithmVersion | Returns the algorithm version of the feature |
ContainerFeature | Returns the container feature for this feature. |
FeatureType | Returns the feature type |
IsContainedFeature | Returns true if the feature is a contained feature. |
IsInternal | Returns true if the feature is internal. |
IsOccurrence | Returns whether this object is an occurrence or not. |
JournalIdentifier | Returns the identifier that would be recorded in a journal for this object. |
Location | Returns the location of the feature |
Name | Returns the custom name of the object. |
OwningComponent | Returns the owning component, if this object is an occurrence. |
OwningPart | Returns the owning part of this object |
Prototype | Returns the prototype of this object if it is an occurrence. |
Suppressed | Returns the suppression status of the feature |
Tag | Returns the Tag for this object. |
Timestamp | Returns the timestamp of the feature |
Methods¶
Method | Description |
---|---|
AddToDieData | Adds the input curves to the die data. |
ChangeBooleanType | Change Boolean Type |
CreateAttributeIterator | Create an attribute iterator @return A new attribute iterator object |
CreateDieData | Creates a copy of the product data in die position. |
DeleteAllAttributesByType | Deletes all attributes of a specific type. |
DeleteAttributeByTypeAndTitle | Deletes an attribute by type and title. |
DeleteClueAlerts | Delete all clue alerts from the features |
DeleteDieData | Deletes the copy of the product data. |
DeleteHintAlerts | Delete all clue alerts from the features |
DeleteInformationalAlerts | Delete all informational alerts from the features |
DeleteUserAttribute | Deletes the first attribute encountered with the given Type, Title. |
DeleteUserAttributes | Deletes the attributes on the object, if any, that satisfy the given iterator |
DeleteWarningAlerts | Delete all warning alerts from the features |
DisplayDieData | Makes the product data in die position visible. |
FindObject | Finds the NXOpen.NXObject with the given identifier as recorded in a journal. |
GetAllChildren | Returns all immediate child features. |
GetAttributeTitlesByType | Gets all the attribute titles of a specific type. |
GetBooleanUserAttribute | Gets a boolean attribute by Title and array Index. |
GetChildren | Returns the immediate child features. |
GetComputationalTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetEntities | Returns the entities created by the feature. |
GetExpressions | Returns the expressions created by the feature. |
GetFeatureClueHintMessages | Returns both clue and hint messages of the feature. |
GetFeatureClueMessages | Returns the feature clue messages. |
GetFeatureColor | The feature color @return |
GetFeatureErrorMessages | Returns the feature error messages. |
GetFeatureHintMessages | Returns the feature hint messages. |
GetFeatureInformationalMessages | Returns the feature informational messages. |
GetFeatureName | Returns the displayed name of the feature. |
GetFeatureWarningMessages | Returns the feature warning messages. |
GetIntegerAttribute | Gets an integer attribute by title. |
GetIntegerUserAttribute | Gets an integer attribute by Title and array Index. |
GetNextUserAttribute | Gets the next attribute encountered on the object, if any, that satisfies the given iterator. |
GetParents | Returns the immediate parent features. |
GetRealAttribute | Gets a real attribute by title. |
GetRealUserAttribute | Gets a real attribute by Title and array Index. |
GetReferenceAttribute | Gets the reference string (not the calculated value) of a string attribute that uses a reference string. |
GetSections | Queries a feature for list of its sections. |
GetStringAttribute | Gets a string attribute value by title. |
GetStringUserAttribute | Gets a string attribute by Title and array Index. |
GetTimeAttribute | Gets a time attribute by title. |
GetTimeUserAttribute | Gets a time attribute by Title and array Index. |
GetUnprocessedHoles | Finds the hole edges that have not been processed yet. |
GetUserAttribute | Gets the first attribute encountered on the object, if any, with a given Title, Type and array Index. |
GetUserAttributeAsString | Gets the first attribute encountered on the object, if any, with a given title, type and array index. |
GetUserAttributeCount | Gets the count of set attributes on the object, if any, that satisfy the given iterator. |
GetUserAttributeLock | Determine the lock of the given attribute. |
GetUserAttributeSize | Gets the size of the first attribute encountered on the object, if any, with a given Title and Type. |
GetUserAttributeSourceObjects | Returns an array of objects from which this object presents attributes. |
GetUserAttributes | Gets all the attributes that have been set on the given object, if any, that satisfy the given iterator. |
GetUserAttributesAsStrings | Gets all the attributes that have been set on the given object. |
HasUserAttribute | Determines if an attribute exists on the object, that satisfies the given iterator @return |
HideBody | Hide the body created by the feature |
HideParents | Hide the body created by the parent feature |
Highlight | Highlight the body created by the feature |
LogDiagnostic | Log a diagnostic alert for this feature |
MakeCurrentFeature | Make current feature |
MakeSketchExternal | Make the parent sketch external for reuse by other features. |
MakeSketchInternal | Make the parent sketch internal if referenced only by this feature. |
MapCollectorToDie | Maps the edges in the collector from part position to die position. |
MapCollectorToPart | Maps the edges in the collector from die position to part position. |
MapEdge | Maps the edge to find the part and die position entity, either can be a None. |
Prints a representation of this object to the system log file. | |
RemoveForEdit | Remove all the feature faces before a NoHistory mode edit. |
RemoveParameters | Remove Local feature parameters in history free mode. |
SetAttribute | Creates or modifies an integer attribute. |
SetBooleanUserAttribute | Creates or modifies a boolean attribute with the option to update or not. |
SetGroupActive | Set a feature group as active group. |
SetName | Sets the custom name of the object. |
SetReferenceAttribute | Creates or modifies a string attribute which uses a reference string. |
SetReferenceCurves | Sets reference curves in the die tip feature. |
SetTimeAttribute | Creates or modifies a time attribute. |
SetTimeUserAttribute | Creates or modifies a time attribute with the option to update or not. |
SetUserAttribute | Creates or modifies an attribute with the option to update or not. |
SetUserAttributeLock | Lock or unlock the given attribute. |
ShowBody | Show the body created by the feature |
ShowDimensions | Show all feature dimensions of a feature. |
ShowParents | Show the body created by the parent feature |
Suppress | Suppress the feature |
TransformDieDirection | Transforms the direction from die position to product position. |
TransformDiePoint | Transforms the point from die position to product position. |
UndisplayDieData | Makes the product data in die position invisible. |
Unhighlight | Unhighlight the body created by the feature |
Unsuppress | Unsuppress the feature |
Property Detail¶
IsOccurrence¶
-
Tip.
IsOccurrence
¶ Returns whether this object is an occurrence or not.
-------------------------------------
Getter Method
Signature
IsOccurrence()
Returns: This object is an occurrence Return type: bool New in version NX3.0.0.
License requirements: None.
JournalIdentifier¶
-
Tip.
JournalIdentifier
¶ Returns the identifier that would be recorded in a journal for this object.
This may not be the same across different releases of the software.
-------------------------------------
Getter Method
Signature
JournalIdentifier()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
Name¶
-
Tip.
Name
¶ Returns the custom name of the object.
-------------------------------------
Getter Method
Signature
Name()
Returns: Return type: str New in version NX3.0.0.
License requirements: None.
OwningComponent¶
-
Tip.
OwningComponent
¶ Returns the owning component, if this object is an occurrence.
-------------------------------------
Getter Method
Signature
OwningComponent()
Returns: Return type: NXOpen.Assemblies.Component
New in version NX3.0.0.
License requirements: None.
OwningPart¶
-
Tip.
OwningPart
¶ Returns the owning part of this object
-------------------------------------
Getter Method
Signature
OwningPart()
Returns: The owning part of this object or null if it does not have an owner Return type: NXOpen.BasePart
New in version NX3.0.0.
License requirements: None.
Prototype¶
-
Tip.
Prototype
¶ Returns the prototype of this object if it is an occurrence.
-------------------------------------
Getter Method
Signature
Prototype()
Returns: The prototype of this object or null if this object is not an occurrence Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
Method Detail¶
AddToDieData¶
-
Tip.
AddToDieData
¶ Adds the input curves to the die data.
Signature
AddToDieData(objects)
Parameters: objects (list of NXOpen.Curve
) – Curves to be added to the die dataNew in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
CreateDieData¶
-
Tip.
CreateDieData
¶ Creates a copy of the product data in die position.
The product data is not visible upon creation. This method must be called before using the methods
Die.Tip.DeleteDieData()
,Die.Tip.DisplayDieData()
,Die.Tip.UndisplayDieData()
,Die.Tip.TransformDiePoint()
, orDie.Tip.TransformDieDirection()
.Signature
CreateDieData(allTips)
Parameters: allTips (bool) – Create the die position product data of all tips in the operation? New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
DeleteDieData¶
-
Tip.
DeleteDieData
¶ Deletes the copy of the product data.
Signature
DeleteDieData()
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
DisplayDieData¶
-
Tip.
DisplayDieData
¶ Makes the product data in die position visible.
The display of the Tip feature is made invisible.
Signature
DisplayDieData()
New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
FindObject¶
-
Tip.
FindObject
¶ Finds the
NXOpen.NXObject
with the given identifier as recorded in a journal.An object may not return the same value as its JournalIdentifier in different versions of the software. However newer versions of the software should find the same object when FindObject is passed older versions of its journal identifier. In general, this method should not be used in handwritten code and exists to support record and playback of journals.
An exception will be thrown if no object can be found with the given journal identifier.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Journal identifier of the object Returns: Return type: NXOpen.INXObject
New in version NX3.0.0.
License requirements: None.
GetUnprocessedHoles¶
-
Tip.
GetUnprocessedHoles
¶ Finds the hole edges that have not been processed yet.
Signature
GetUnprocessedHoles()
Returns: Return type: list of NXOpen.Edge
New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MapCollectorToDie¶
-
Tip.
MapCollectorToDie
¶ Maps the edges in the collector from part position to die position.
Signature
MapCollectorToDie(collector)
Parameters: collector ( NXOpen.ScCollector
) –New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MapCollectorToPart¶
-
Tip.
MapCollectorToPart
¶ Maps the edges in the collector from die position to part position.
Signature
MapCollectorToPart(collector)
Parameters: collector ( NXOpen.ScCollector
) –New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
MapEdge¶
-
Tip.
MapEdge
¶ Maps the edge to find the part and die position entity, either can be a None.
Signature
MapEdge(inEdge)
Parameters: inEdge ( NXOpen.IProfile
) –Returns: a tuple Return type: A tuple consisting of (partEdge, dieEdge). partEdge is a NXOpen.IProfile
. dieEdge is aNXOpen.IProfile
.New in version NX5.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
Print¶
-
Tip.
Print
¶ Prints a representation of this object to the system log file.
Signature
Print()
New in version NX3.0.0.
License requirements: None.
SetName¶
-
Tip.
SetName
¶ Sets the custom name of the object.
NOTE: This method should not be used to edit a read-only object such as a Mirrored PMI object. If it is, the changes will be overridden when the part is updated.
Signature
SetName(name)
Parameters: name (str) – New in version NX3.0.0.
License requirements: None.
SetReferenceCurves¶
-
Tip.
SetReferenceCurves
¶ Sets reference curves in the die tip feature.
Signature
SetReferenceCurves(objects)
Parameters: objects (list of NXOpen.Curve
) – Curves to be added to the tipNew in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TransformDieDirection¶
-
Tip.
TransformDieDirection
¶ Transforms the direction from die position to product position.
Signature
TransformDieDirection(vector)
Parameters: vector ( NXOpen.Direction
) – Direction to be transformed.New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)
TransformDiePoint¶
-
Tip.
TransformDiePoint
¶ Transforms the point from die position to product position.
Signature
TransformDiePoint(point)
Parameters: point ( NXOpen.Point
) – Point to be transformed.New in version NX4.0.0.
License requirements: die_engineering (“DIE ENGINEERING”)