ThroatParentBuilderTypeOption Enumeration

NXOpen.Die.ThroatParentBuilder.TypeOption is an alias for NXOpen.Die.ThroatParentBuilderTypeOption

class NXOpen.Die.ThroatParentBuilderTypeOption

Bases: object

Settings for the type of the throat section.

Enum Members

Enum Member Enum Member Description
Wipe
Throat is built for a wipe operation.
Restrike
Throat is built for a restrike operation.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.