SteelInsertSegmentParentBuilder Class¶
-
class
NXOpen.Die.
SteelInsertSegmentParentBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Steel Insert Segment Parent sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
AddEndPointsSwitch | Returns or sets the add end points switch |
BeltThickness | Returns the belt thickness |
BuildStatus | Returns the build status of die sisegs |
DesignStatus | Returns or sets the design status of die sisegs |
DisplayStatus | Returns or sets the display status of die sisegs |
ExtensionDistance | Returns the extension distance |
ExtensionType | Returns or sets the extension type |
InsertType | Returns or sets the insert type |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProfileRelief | Returns the profile relief |
ProfileReliefToggle | Returns or sets the profile relief |
ReliefAngle | Returns the relief angle |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreateChild | Creates a child siseg @return |
DeleteChild | Deletes a child siseg |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetChildren | Outputs the children @return children |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetBeltThickness | |
SetExtensionDistance | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetProfileRelief | |
SetReliefAngle | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Enumerations¶
SteelInsertSegmentParentBuilderExtensionTypeOption Enumeration | Settings for the extension type. |
SteelInsertSegmentParentBuilderInsertTypeOption Enumeration | Settings for the insert type. |
Property Detail¶
AddEndPointsSwitch¶
-
SteelInsertSegmentParentBuilder.
AddEndPointsSwitch
¶ Returns or sets the add end points switch
-------------------------------------
Getter Method
Signature
AddEndPointsSwitch()
Returns: Return type: int New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
AddEndPointsSwitch(addEndPointsSwitch)
Parameters: addEndPointsSwitch (int) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BeltThickness¶
-
SteelInsertSegmentParentBuilder.
BeltThickness
¶ Returns the belt thickness
-------------------------------------
Getter Method
Signature
BeltThickness()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BuildStatus¶
-
SteelInsertSegmentParentBuilder.
BuildStatus
¶ Returns the build status of die sisegs
-------------------------------------
Getter Method
Signature
BuildStatus()
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
SteelInsertSegmentParentBuilder.
DesignStatus
¶ Returns or sets the design status of die sisegs
-------------------------------------
Getter Method
Signature
DesignStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus(designStatus)
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
SteelInsertSegmentParentBuilder.
DisplayStatus
¶ Returns or sets the display status of die sisegs
-------------------------------------
Getter Method
Signature
DisplayStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus(displayStatus)
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ExtensionDistance¶
-
SteelInsertSegmentParentBuilder.
ExtensionDistance
¶ Returns the extension distance
-------------------------------------
Getter Method
Signature
ExtensionDistance()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ExtensionType¶
-
SteelInsertSegmentParentBuilder.
ExtensionType
¶ Returns or sets the extension type
-------------------------------------
Getter Method
Signature
ExtensionType()
Returns: Return type: NXOpen.Die.SteelInsertSegmentParentBuilderExtensionTypeOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
ExtensionType(extensionType)
Parameters: extensionType ( NXOpen.Die.SteelInsertSegmentParentBuilderExtensionTypeOption
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
InsertType¶
-
SteelInsertSegmentParentBuilder.
InsertType
¶ Returns or sets the insert type
-------------------------------------
Getter Method
Signature
InsertType()
Returns: Return type: NXOpen.Die.SteelInsertSegmentParentBuilderInsertTypeOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
InsertType(insertType)
Parameters: insertType ( NXOpen.Die.SteelInsertSegmentParentBuilderInsertTypeOption
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ProfileRelief¶
-
SteelInsertSegmentParentBuilder.
ProfileRelief
¶ Returns the profile relief
-------------------------------------
Getter Method
Signature
ProfileRelief()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ProfileReliefToggle¶
-
SteelInsertSegmentParentBuilder.
ProfileReliefToggle
¶ Returns or sets the profile relief
-------------------------------------
Getter Method
Signature
ProfileReliefToggle()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
ProfileReliefToggle(profileReliefToggle)
Parameters: profileReliefToggle (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ReliefAngle¶
-
SteelInsertSegmentParentBuilder.
ReliefAngle
¶ Returns the relief angle
-------------------------------------
Getter Method
Signature
ReliefAngle()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
CreateChild¶
-
SteelInsertSegmentParentBuilder.
CreateChild
¶ Creates a child siseg
Signature
CreateChild()
Returns: Return type: NXOpen.Die.SteelInsertSegmentChildBuilder
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DeleteChild¶
-
SteelInsertSegmentParentBuilder.
DeleteChild
¶ Deletes a child siseg
Signature
DeleteChild(diesisegchild)
Parameters: diesisegchild ( NXOpen.Die.SteelInsertSegmentChildBuilder
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetChildren¶
-
SteelInsertSegmentParentBuilder.
GetChildren
¶ Outputs the children
Signature
GetChildren()
Returns: children Return type: list of NXOpen.Die.SteelInsertSegmentChildBuilder
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBeltThickness¶
-
SteelInsertSegmentParentBuilder.
SetBeltThickness
¶ Signature
SetBeltThickness(beltThickness)
Parameters: beltThickness (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetExtensionDistance¶
-
SteelInsertSegmentParentBuilder.
SetExtensionDistance
¶ Signature
SetExtensionDistance(extensionDistance)
Parameters: extensionDistance (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetProfileRelief¶
-
SteelInsertSegmentParentBuilder.
SetProfileRelief
¶ Signature
SetProfileRelief(profileRelief)
Parameters: profileRelief (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetReliefAngle¶
-
SteelInsertSegmentParentBuilder.
SetReliefAngle
¶ Signature
SetReliefAngle(reliefAngle)
Parameters: reliefAngle (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
SteelInsertSegmentParentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.