SteelInsertSegmentChildBuilderExtensionTypeOption Enumeration¶
NXOpen.Die.SteelInsertSegmentChildBuilder.ExtensionTypeOption is an alias for NXOpen.Die.SteelInsertSegmentChildBuilderExtensionTypeOption
-
class
NXOpen.Die.
SteelInsertSegmentChildBuilderExtensionTypeOption
¶ Bases:
object
Settings for the extension type.
Enum Members
Enum Member Enum Member Description Constant constantMaxdistPlusConst maximum distance + constantLaw law-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-