SteelInsertSectionBuilderExtensionTypeOption Enumeration

NXOpen.Die.SteelInsertSectionBuilder.ExtensionTypeOption is an alias for NXOpen.Die.SteelInsertSectionBuilderExtensionTypeOption

class NXOpen.Die.SteelInsertSectionBuilderExtensionTypeOption

Bases: object

Settings for the extension type.

Enum Members

Enum Member Enum Member Description
Constant
constant
MaxdistPlusConst
maximum distance + constant
Law
law
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.