SteelInsertBuilderInsertTypeOption Enumeration

NXOpen.Die.SteelInsertBuilder.InsertTypeOption is an alias for NXOpen.Die.SteelInsertBuilderInsertTypeOption

class NXOpen.Die.SteelInsertBuilderInsertTypeOption

Bases: object

Settings for the insert type.

Enum Members

Enum Member Enum Member Description
Trim
trim
Flange
flange
OffsetFlange
offset_flange
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.