SpringbackCompensationBuilderResultSheetType Enumeration

NXOpen.Die.SpringbackCompensationBuilder.ResultSheetType is an alias for NXOpen.Die.SpringbackCompensationBuilderResultSheetType

class NXOpen.Die.SpringbackCompensationBuilderResultSheetType

Bases: object

The type of sheet body you would like created as output.

Enum Members

Enum Member Enum Member Description
Compensated
Compensated sheet body.
Sprung
Sprung sheet body.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.