SpringbackCompensationBuilderDegreeType Enumeration

NXOpen.Die.SpringbackCompensationBuilder.DegreeType is an alias for NXOpen.Die.SpringbackCompensationBuilderDegreeType

class NXOpen.Die.SpringbackCompensationBuilderDegreeType

Bases: object

The polynomial degree type.

Acceptable degrees are 2, 3, 5, and 7.

Enum Members

Enum Member Enum Member Description
Two
Degree is 2
Three
Degree is 3
Five
Degree is 5
Seven
Degree is 7
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.