QuickBinderBuilderTypes Enumeration

NXOpen.Die.QuickBinderBuilder.Types is an alias for NXOpen.Die.QuickBinderBuilderTypes

class NXOpen.Die.QuickBinderBuilderTypes

Bases: object

The method used to approximate the product faces.

Enum Members

Enum Member Enum Member Description
Planar
planar
Cylindrical
cylindrical
Conical
conical
MonoArc
mono arc
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.