PressureSystemParentBuilder Class

class NXOpen.Die.PressureSystemParentBuilder

Bases: NXOpen.Features.FeatureBuilder

Represents a Die Pressure System Parent sub feature.

This sub feature is created via the main feature builder.

New in version NX4.0.0.

Properties

Property Description
BuildStatus Returns the build status of pressure systems.
Clearance Returns or sets the clearance of pressure systems.
DesignStatus Returns or sets the design status of pressure systems, if true the pressure systems will be built into the model, if false they will not.
Diameter Returns or sets the diameter of pressure systems.
DisplayStatus Returns or sets the display status of pressure systems, if true input data to the pressure systems will be displayed, if false the input data will not be displayed.
Height Returns or sets the height of pressure systems.
ParentFeatureInternal Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal
PatchSolutionFlag Returns or sets the patch solution flag
PatchSurfaceFilename Returns or sets the patch surface filename
SurroundingPatchSurfaceFilename Returns or sets the surrounding patch surface filename
Tag Returns the Tag for this object.
XCount Returns or sets the x count of pressure systems.
XDistance Returns or sets the x distance of pressure systems.
XOffset Returns or sets the x offset of pressure systems.
YCount Returns or sets the y count of pressure systems.
YDistance Returns or sets the y distance of pressure systems.
YOffset Returns or sets the y offset of pressure systems.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
CommitFeature Commits the feature parameters and creates the feature @return
CreateChild Creates a child pressure system.
DeleteChild Deletes a child pressure system.
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetChildren Outputs the child pressure systems.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetFeature Returns the feature currently being edited by this builder.
GetObject Returns the object currently being edited by this builder.
HideInternalParentFeatureAfterEdit Re-suppress an internal parent feature (a slave feature) after it has been edited.
SetParentFeatureInternal Set the parent features which would be internal or slaves to the feature being created or commited
ShowInternalParentFeatureForEdit Unsuppress an internal parent feature (a slave feature) so it can be edited.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
UnsetParentFeatureInternal Set the internal parent feature of the feature being edited to external
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

BuildStatus

PressureSystemParentBuilder.BuildStatus

Returns the build status of pressure systems.

-------------------------------------

Getter Method

Signature BuildStatus()

Returns:
Return type:NXOpen.Die.DieBuildStatusOption

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Clearance

PressureSystemParentBuilder.Clearance

Returns or sets the clearance of pressure systems.

-------------------------------------

Getter Method

Signature Clearance()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Clearance(clearance)

Parameters:clearance (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

DesignStatus

PressureSystemParentBuilder.DesignStatus

Returns or sets the design status of pressure systems, if true the pressure systems will be built into the model, if false they will not.

-------------------------------------

Getter Method

Signature DesignStatus()

Returns:
Return type:bool

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature DesignStatus(designStatus)

Parameters:designStatus (bool) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Diameter

PressureSystemParentBuilder.Diameter

Returns or sets the diameter of pressure systems.

-------------------------------------

Getter Method

Signature Diameter()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Diameter(diameter)

Parameters:diameter (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

DisplayStatus

PressureSystemParentBuilder.DisplayStatus

Returns or sets the display status of pressure systems, if true input data to the pressure systems will be displayed, if false the input data will not be displayed.

-------------------------------------

Getter Method

Signature DisplayStatus()

Returns:
Return type:bool

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature DisplayStatus(displayStatus)

Parameters:displayStatus (bool) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Height

PressureSystemParentBuilder.Height

Returns or sets the height of pressure systems.

-------------------------------------

Getter Method

Signature Height()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Height(height)

Parameters:height (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

XCount

PressureSystemParentBuilder.XCount

Returns or sets the x count of pressure systems.

-------------------------------------

Getter Method

Signature XCount()

Returns:
Return type:int

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature XCount(xCount)

Parameters:xCount (int) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

XDistance

PressureSystemParentBuilder.XDistance

Returns or sets the x distance of pressure systems.

-------------------------------------

Getter Method

Signature XDistance()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature XDistance(xDistance)

Parameters:xDistance (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

XOffset

PressureSystemParentBuilder.XOffset

Returns or sets the x offset of pressure systems.

-------------------------------------

Getter Method

Signature XOffset()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature XOffset(xOffset)

Parameters:xOffset (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

YCount

PressureSystemParentBuilder.YCount

Returns or sets the y count of pressure systems.

-------------------------------------

Getter Method

Signature YCount()

Returns:
Return type:int

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature YCount(yCount)

Parameters:yCount (int) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

YDistance

PressureSystemParentBuilder.YDistance

Returns or sets the y distance of pressure systems.

-------------------------------------

Getter Method

Signature YDistance()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature YDistance(yDistance)

Parameters:yDistance (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

YOffset

PressureSystemParentBuilder.YOffset

Returns or sets the y offset of pressure systems.

-------------------------------------

Getter Method

Signature YOffset()

Returns:
Return type:float

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature YOffset(yOffset)

Parameters:yOffset (float) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Method Detail

CreateChild

PressureSystemParentBuilder.CreateChild

Creates a child pressure system.

Signature CreateChild()

Returns:
Return type:NXOpen.Die.PressureSystemChildBuilder

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

DeleteChild

PressureSystemParentBuilder.DeleteChild

Deletes a child pressure system.

Signature DeleteChild(diepressuresystemchild)

Parameters:diepressuresystemchild (NXOpen.Die.PressureSystemChildBuilder) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

GetChildren

PressureSystemParentBuilder.GetChildren

Outputs the child pressure systems.

Signature GetChildren()

Returns:The child pressure systems.
Return type:list of NXOpen.Die.PressureSystemChildBuilder

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Validate

PressureSystemParentBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.