PressModel Class

class NXOpen.Die.PressModel

Bases: NXOpen.TransientObject

Represents a Die Simulation - Press Model

New in version NX6.0.0.

Methods

Method Description
Dispose Frees the object from memory.
GetNumOperations Get number of operations @return
SetOperationCushionSettings Set operation cushion values
SetOperationSlideHeight Set operation slide height
SetOperationTransportCurveSet Tell the press model which transport curve set to use in the given operation
SetOperationUserTransportCurves Set values of the User Defined transport curve set, for given operation

Method Detail

Dispose

PressModel.Dispose

Frees the object from memory.

After this method is called, it is illegal to use the object. In .NET, this method is automatically called when the object is deleted by the garbage collector.

Signature Dispose()

New in version NX6.0.0.

License requirements: None.

GetNumOperations

PressModel.GetNumOperations

Get number of operations

Signature GetNumOperations()

Returns:
Return type:int

New in version NX6.0.0.

License requirements: ug_die_design (“Die Design”)

SetOperationCushionSettings

PressModel.SetOperationCushionSettings

Set operation cushion values

Signature SetOperationCushionSettings(operation, liftStartAngle, liftStopAngle, liftToDist, lockAtDist)

Parameters:
  • operation (int) – Operation of the cushion
  • liftStartAngle (float) – Lift start angle
  • liftStopAngle (float) – Lift stop angle
  • liftToDist (float) – Distance to lift to
  • lockAtDist (float) – Distance where lock happens

New in version NX6.0.0.

License requirements: ug_die_design (“Die Design”)

SetOperationSlideHeight

PressModel.SetOperationSlideHeight

Set operation slide height

Signature SetOperationSlideHeight(operation, slideHeight)

Parameters:
  • operation (int) – Operation of the slide
  • slideHeight (float) – Slide height

New in version NX6.0.0.

License requirements: ug_die_design (“Die Design”)

SetOperationTransportCurveSet

PressModel.SetOperationTransportCurveSet

Tell the press model which transport curve set to use in the given operation

Signature SetOperationTransportCurveSet(operation, curveSet)

Parameters:
  • operation (int) – Operation of the transport devices
  • curveSet (int) – Index of the curve set

New in version NX6.0.0.

License requirements: ug_die_design (“Die Design”)

SetOperationUserTransportCurves

PressModel.SetOperationUserTransportCurves

Set values of the User Defined transport curve set, for given operation

Signature SetOperationUserTransportCurves(operation, vals)

Parameters:
  • operation (int) – Operation of the transport devices
  • vals (list of float) – The curve set values

New in version NX6.0.0.

License requirements: ug_die_design (“Die Design”)