PointChildBuilder Class

class NXOpen.Die.PointChildBuilder

Bases: NXOpen.Features.FeatureBuilder

Represents a Die Point Child sub feature.

This sub feature is created via the main feature builder.

New in version NX4.0.0.

Properties

Property Description
BuildStatus Returns the build status of the point.
DesignStatus Returns or sets the design status of the point, if true the point will be built into the model, if false it will not.
DisplayStatus Returns or sets the display status of the point, if true input data to the point will be displayed, if false the input data will not be displayed.
ParentFeatureInternal Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal
PatchSolutionFlag Returns or sets the patch solution flag
PatchSurfaceFilename Returns or sets the patch surface filename
Point Returns or sets the location of the point.
SurroundingPatchSurfaceFilename Returns or sets the surrounding patch surface filename
Tag Returns the Tag for this object.

Methods

Method Description
Commit Commits any edits that have been applied to the builder.
CommitFeature Commits the feature parameters and creates the feature @return
Destroy Deletes the builder, and cleans up any objects created by the builder.
GetCommittedObjects For builders that create more than one object, this method returns the objects that are created by commit.
GetFeature Returns the feature currently being edited by this builder.
GetObject Returns the object currently being edited by this builder.
HideInternalParentFeatureAfterEdit Re-suppress an internal parent feature (a slave feature) after it has been edited.
SetParentFeatureInternal Set the parent features which would be internal or slaves to the feature being created or commited
ShowInternalParentFeatureForEdit Unsuppress an internal parent feature (a slave feature) so it can be edited.
ShowResults Updates the model to reflect the result of an edit to the model for all builders that support showing results.
UnsetParentFeatureInternal Set the internal parent feature of the feature being edited to external
Validate Validate whether the inputs to the component are sufficient for commit to be called.

Property Detail

BuildStatus

PointChildBuilder.BuildStatus

Returns the build status of the point.

-------------------------------------

Getter Method

Signature BuildStatus()

Returns:
Return type:NXOpen.Die.DieBuildStatusOption

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

DesignStatus

PointChildBuilder.DesignStatus

Returns or sets the design status of the point, if true the point will be built into the model, if false it will not.

-------------------------------------

Getter Method

Signature DesignStatus()

Returns:
Return type:bool

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature DesignStatus(designStatus)

Parameters:designStatus (bool) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

DisplayStatus

PointChildBuilder.DisplayStatus

Returns or sets the display status of the point, if true input data to the point will be displayed, if false the input data will not be displayed.

-------------------------------------

Getter Method

Signature DisplayStatus()

Returns:
Return type:bool

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature DisplayStatus(displayStatus)

Parameters:displayStatus (bool) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Point

PointChildBuilder.Point

Returns or sets the location of the point.

-------------------------------------

Getter Method

Signature Point()

Returns:
Return type:NXOpen.Point

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

-------------------------------------

Setter Method

Signature Point(point)

Parameters:point (NXOpen.Point) –

New in version NX4.0.0.

License requirements: ug_die_design (“Die Design”)

Method Detail

Validate

PointChildBuilder.Validate

Validate whether the inputs to the component are sufficient for commit to be called.

If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.

Signature Validate()

Returns:Was self validation successful
Return type:bool

New in version NX3.0.1.

License requirements: None.