PierceHoleParentBuilder Class¶
-
class
NXOpen.Die.
PierceHoleParentBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Pierce Hole Parent sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
BreakerHoleDepth | Returns the breaker hole depth of pierce holes |
BreakerHoleFactor | Returns the breaker hole factor of pierce holes |
BreakerHoleOffset | Returns the breaker hole offset of pierce holes |
BuildStatus | Returns the build status of pierce holes |
CircularSlugHole | Returns or sets the circular slug hole switch of pierce holes |
CommonSlugHole | Returns or sets the common slug hole switch of pierce holes |
Depth | Returns the depth of pierce holes |
DesignStatus | Returns or sets the design status of pierce holes |
Diameter | Returns the diameter of pierce holes |
DieClearance | Returns the die clearance of pierce holes |
DisplayHoles | Returns or sets the display holes option of pierce holes |
DisplayStatus | Returns or sets the display status of pierce holes |
Length | Returns the length of pierce holes |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
ProfileBlendRadius | Returns the profile blend radius of pierce holes |
SlugHoleDiameterIncrement | Returns the slug hole diameter increment of pierce holes |
SlugHoleOffset | Returns the slug hole offset of pierce holes |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Width | Returns the width of pierce holes |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
CreateChild | Creates a child pierce hole @return |
DeleteChild | Deletes a child pierce hole |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetBreakerHoleAttributes | Gets the breaker hole attributes, note existance of attributes depends on usage in main feature |
GetChildren | Outputs the pierce hole children @return children |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetHoleAttributes | Gets the hole attributes, note existance of attributes depends on usage in main feature |
GetObject | Returns the object currently being edited by this builder. |
GetSlugHoleAttributes | Gets the slug hole attributes, note existance of attributes depends on usage in main feature |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetBreakerHoleAttributes | Sets the breaker hole attributes, note existance of attributes depends on usage in main feature |
SetBreakerHoleDepth | |
SetBreakerHoleFactor | |
SetBreakerHoleOffset | |
SetDepth | |
SetDiameter | |
SetDieClearance | |
SetHoleAttributes | Sets the hole attributes, note existance of attributes depends on usage in main feature |
SetLength | |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
SetProfileBlendRadius | |
SetSlugHoleAttributes | Sets the slug hole attributes, note existance of attributes depends on usage in main feature |
SetSlugHoleDiameterIncrement | |
SetSlugHoleOffset | |
SetWidth | |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
BreakerHoleDepth¶
-
PierceHoleParentBuilder.
BreakerHoleDepth
¶ Returns the breaker hole depth of pierce holes
-------------------------------------
Getter Method
Signature
BreakerHoleDepth()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BreakerHoleFactor¶
-
PierceHoleParentBuilder.
BreakerHoleFactor
¶ Returns the breaker hole factor of pierce holes
-------------------------------------
Getter Method
Signature
BreakerHoleFactor()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BreakerHoleOffset¶
-
PierceHoleParentBuilder.
BreakerHoleOffset
¶ Returns the breaker hole offset of pierce holes
-------------------------------------
Getter Method
Signature
BreakerHoleOffset()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BuildStatus¶
-
PierceHoleParentBuilder.
BuildStatus
¶ Returns the build status of pierce holes
-------------------------------------
Getter Method
Signature
BuildStatus()
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
CircularSlugHole¶
-
PierceHoleParentBuilder.
CircularSlugHole
¶ Returns or sets the circular slug hole switch of pierce holes
-------------------------------------
Getter Method
Signature
CircularSlugHole()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
CircularSlugHole(circularSlugHole)
Parameters: circularSlugHole (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
CommonSlugHole¶
-
PierceHoleParentBuilder.
CommonSlugHole
¶ Returns or sets the common slug hole switch of pierce holes
-------------------------------------
Getter Method
Signature
CommonSlugHole()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
CommonSlugHole(commonSlugHole)
Parameters: commonSlugHole (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Depth¶
-
PierceHoleParentBuilder.
Depth
¶ Returns the depth of pierce holes
-------------------------------------
Getter Method
Signature
Depth()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
PierceHoleParentBuilder.
DesignStatus
¶ Returns or sets the design status of pierce holes
-------------------------------------
Getter Method
Signature
DesignStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus(designStatus)
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Diameter¶
-
PierceHoleParentBuilder.
Diameter
¶ Returns the diameter of pierce holes
-------------------------------------
Getter Method
Signature
Diameter()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DieClearance¶
-
PierceHoleParentBuilder.
DieClearance
¶ Returns the die clearance of pierce holes
-------------------------------------
Getter Method
Signature
DieClearance()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayHoles¶
-
PierceHoleParentBuilder.
DisplayHoles
¶ Returns or sets the display holes option of pierce holes
-------------------------------------
Getter Method
Signature
DisplayHoles()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayHoles(displayPierceHoles)
Parameters: displayPierceHoles (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
PierceHoleParentBuilder.
DisplayStatus
¶ Returns or sets the display status of pierce holes
-------------------------------------
Getter Method
Signature
DisplayStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus(displayStatus)
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Length¶
-
PierceHoleParentBuilder.
Length
¶ Returns the length of pierce holes
-------------------------------------
Getter Method
Signature
Length()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ProfileBlendRadius¶
-
PierceHoleParentBuilder.
ProfileBlendRadius
¶ Returns the profile blend radius of pierce holes
-------------------------------------
Getter Method
Signature
ProfileBlendRadius()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SlugHoleDiameterIncrement¶
-
PierceHoleParentBuilder.
SlugHoleDiameterIncrement
¶ Returns the slug hole diameter increment of pierce holes
-------------------------------------
Getter Method
Signature
SlugHoleDiameterIncrement()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SlugHoleOffset¶
-
PierceHoleParentBuilder.
SlugHoleOffset
¶ Returns the slug hole offset of pierce holes
-------------------------------------
Getter Method
Signature
SlugHoleOffset()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Width¶
-
PierceHoleParentBuilder.
Width
¶ Returns the width of pierce holes
-------------------------------------
Getter Method
Signature
Width()
Returns: Return type: NXOpen.Expression
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
CreateChild¶
-
PierceHoleParentBuilder.
CreateChild
¶ Creates a child pierce hole
Signature
CreateChild()
Returns: Return type: NXOpen.Die.PierceHoleChildBuilder
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DeleteChild¶
-
PierceHoleParentBuilder.
DeleteChild
¶ Deletes a child pierce hole
Signature
DeleteChild(dieholechild)
Parameters: dieholechild ( NXOpen.Die.PierceHoleChildBuilder
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetBreakerHoleAttributes¶
-
PierceHoleParentBuilder.
GetBreakerHoleAttributes
¶ Gets the breaker hole attributes, note existance of attributes depends on usage in main feature
Signature
GetBreakerHoleAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color, diameterTitle). title is a str. title for attribute value is a str. value of attribute color is a int. color of hole faces diameterTitle is a str. title for diameter attribute New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetChildren¶
-
PierceHoleParentBuilder.
GetChildren
¶ Outputs the pierce hole children
Signature
GetChildren()
Returns: children Return type: list of NXOpen.Die.PierceHoleChildBuilder
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetHoleAttributes¶
-
PierceHoleParentBuilder.
GetHoleAttributes
¶ Gets the hole attributes, note existance of attributes depends on usage in main feature
Signature
GetHoleAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color, diameterTitle). title is a str. title for attribute value is a str. value of attribute color is a int. color of hole faces diameterTitle is a str. title for diameter attribute New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
GetSlugHoleAttributes¶
-
PierceHoleParentBuilder.
GetSlugHoleAttributes
¶ Gets the slug hole attributes, note existance of attributes depends on usage in main feature
Signature
GetSlugHoleAttributes()
Returns: a tuple Return type: A tuple consisting of (title, value, color, diameterTitle). title is a str. title for attribute value is a str. value of attribute color is a int. color of hole faces diameterTitle is a str. title for diameter attribute New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBreakerHoleAttributes¶
-
PierceHoleParentBuilder.
SetBreakerHoleAttributes
¶ Sets the breaker hole attributes, note existance of attributes depends on usage in main feature
Signature
SetBreakerHoleAttributes(title, value, color, diameterTitle)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of hole faces
- diameterTitle (str) – title for diameter attribute
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBreakerHoleDepth¶
-
PierceHoleParentBuilder.
SetBreakerHoleDepth
¶ Signature
SetBreakerHoleDepth(breakerHoleDepth)
Parameters: breakerHoleDepth (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBreakerHoleFactor¶
-
PierceHoleParentBuilder.
SetBreakerHoleFactor
¶ Signature
SetBreakerHoleFactor(breakerHoleFactor)
Parameters: breakerHoleFactor (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetBreakerHoleOffset¶
-
PierceHoleParentBuilder.
SetBreakerHoleOffset
¶ Signature
SetBreakerHoleOffset(breakerHoleOffset)
Parameters: breakerHoleOffset (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetDepth¶
-
PierceHoleParentBuilder.
SetDepth
¶ Signature
SetDepth(depth)
Parameters: depth (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetDiameter¶
-
PierceHoleParentBuilder.
SetDiameter
¶ Signature
SetDiameter(diameter)
Parameters: diameter (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetDieClearance¶
-
PierceHoleParentBuilder.
SetDieClearance
¶ Signature
SetDieClearance(dieClearance)
Parameters: dieClearance (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetHoleAttributes¶
-
PierceHoleParentBuilder.
SetHoleAttributes
¶ Sets the hole attributes, note existance of attributes depends on usage in main feature
Signature
SetHoleAttributes(title, value, color, diameterTitle)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of hole faces
- diameterTitle (str) – title for diameter attribute
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetLength¶
-
PierceHoleParentBuilder.
SetLength
¶ Signature
SetLength(length)
Parameters: length (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetProfileBlendRadius¶
-
PierceHoleParentBuilder.
SetProfileBlendRadius
¶ Signature
SetProfileBlendRadius(profileBlendRadius)
Parameters: profileBlendRadius (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetSlugHoleAttributes¶
-
PierceHoleParentBuilder.
SetSlugHoleAttributes
¶ Sets the slug hole attributes, note existance of attributes depends on usage in main feature
Signature
SetSlugHoleAttributes(title, value, color, diameterTitle)
Parameters: - title (str) – title for attribute
- value (str) – value of attribute
- color (int) – color of hole faces
- diameterTitle (str) – title for diameter attribute
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetSlugHoleDiameterIncrement¶
-
PierceHoleParentBuilder.
SetSlugHoleDiameterIncrement
¶ Signature
SetSlugHoleDiameterIncrement(slugHoleDiameterIncrement)
Parameters: slugHoleDiameterIncrement (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetSlugHoleOffset¶
-
PierceHoleParentBuilder.
SetSlugHoleOffset
¶ Signature
SetSlugHoleOffset(slugHoleOffset)
Parameters: slugHoleOffset (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SetWidth¶
-
PierceHoleParentBuilder.
SetWidth
¶ Signature
SetWidth(pierceHoleWidth)
Parameters: pierceHoleWidth (str) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Validate¶
-
PierceHoleParentBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.