PadChildBuilderShapeTypeOption Enumeration

NXOpen.Die.PadChildBuilder.ShapeTypeOption is an alias for NXOpen.Die.PadChildBuilderShapeTypeOption

class NXOpen.Die.PadChildBuilderShapeTypeOption

Bases: object

Settings for the shape type of the die pad.

Enum Members

Enum Member Enum Member Description
Rectangular
Rectangular pad.
Circular
Circular pad.
Curve
Curve defined pad.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.