KeywayChildBuilderRunoffTypeOption Enumeration

NXOpen.Die.KeywayChildBuilder.RunoffTypeOption is an alias for NXOpen.Die.KeywayChildBuilderRunoffTypeOption

class NXOpen.Die.KeywayChildBuilderRunoffTypeOption

Bases: object

Settings for the runoff type of the keyway.

Enum Members

Enum Member Enum Member Description
Rectangular
Rectangular runoff.
Circular
Circular runoff.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.