HandlingCoreBuilderTypes Enumeration

NXOpen.Die.HandlingCoreBuilder.Types is an alias for NXOpen.Die.HandlingCoreBuilderTypes

class NXOpen.Die.HandlingCoreBuilderTypes

Bases: object

Identifies how the handling Core is located in space.

Enum Members

Enum Member Enum Member Description
AtLocation
Location specified by the user.
FromBase
Location is an offset from the base.
MapFromBase
Locate by finding the minimum distance to the main profile of the target and then project and offset from the base. Used specifically for coring the main wall.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.