FlangeTaskBuilderSpringbackTypes Enumeration

NXOpen.Die.FlangeTaskBuilder.SpringbackTypes is an alias for NXOpen.Die.FlangeTaskBuilderSpringbackTypes

class NXOpen.Die.FlangeTaskBuilderSpringbackTypes

Bases: object

Settings for the springback type of the flange task.

Enum Members

Enum Member Enum Member Description
Constant
Constant
Law
Law Controlled
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.