FlangeSteelRibChildBuilder Class¶
-
class
NXOpen.Die.
FlangeSteelRibChildBuilder
¶ Bases:
NXOpen.Features.FeatureBuilder
Represents a Die Flange Steel Rib Child sub feature.
This sub feature is created via the main feature builder.
New in version NX4.0.0.
Properties¶
Property | Description |
---|---|
Angle | Returns or sets the angle of the Flange Steel Rib |
BackDistance | Returns or sets the back distance of the Flange Steel Rib |
BuildStatus | Returns the build status of the Flange Steel Rib |
ChamferDistance | Returns or sets the chamfer distance of the Flange Steel Rib |
DesignStatus | Returns or sets the design status of the Flange Steel Rib |
DisplayStatus | Returns or sets the display status of the Flange Steel Rib |
Offset | Returns or sets the offset of the Flange Steel Rib |
ParentFeatureInternal | Returns or sets whether or not the latest timestamped parent feature of this feature should be made internal |
PatchSolutionFlag | Returns or sets the patch solution flag |
PatchSurfaceFilename | Returns or sets the patch surface filename |
Plane | Returns or sets the plane of the Flange Steel Rib |
SheetMetalDistance | Returns or sets the sheet metal distance of the Flange Steel Rib |
SurroundingPatchSurfaceFilename | Returns or sets the surrounding patch surface filename |
Tag | Returns the Tag for this object. |
Thickness | Returns or sets the thickness of the Flange Steel Rib |
UseAngle | Returns or sets the use angle toggle of the Flange Steel Ribs |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
CommitFeature | Commits the feature parameters and creates the feature @return |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetFeature | Returns the feature currently being edited by this builder. |
GetObject | Returns the object currently being edited by this builder. |
HideInternalParentFeatureAfterEdit | Re-suppress an internal parent feature (a slave feature) after it has been edited. |
SetParentFeatureInternal | Set the parent features which would be internal or slaves to the feature being created or commited |
ShowInternalParentFeatureForEdit | Unsuppress an internal parent feature (a slave feature) so it can be edited. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
UnsetParentFeatureInternal | Set the internal parent feature of the feature being edited to external |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
Angle¶
-
FlangeSteelRibChildBuilder.
Angle
¶ Returns or sets the angle of the Flange Steel Rib
-------------------------------------
Getter Method
Signature
Angle()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Angle(angle)
Parameters: angle (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BackDistance¶
-
FlangeSteelRibChildBuilder.
BackDistance
¶ Returns or sets the back distance of the Flange Steel Rib
-------------------------------------
Getter Method
Signature
BackDistance()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
BackDistance(backDistance)
Parameters: backDistance (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
BuildStatus¶
-
FlangeSteelRibChildBuilder.
BuildStatus
¶ Returns the build status of the Flange Steel Rib
-------------------------------------
Getter Method
Signature
BuildStatus()
Returns: Return type: NXOpen.Die.DieBuildStatusOption
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
ChamferDistance¶
-
FlangeSteelRibChildBuilder.
ChamferDistance
¶ Returns or sets the chamfer distance of the Flange Steel Rib
-------------------------------------
Getter Method
Signature
ChamferDistance()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
ChamferDistance(chamferDistance)
Parameters: chamferDistance (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DesignStatus¶
-
FlangeSteelRibChildBuilder.
DesignStatus
¶ Returns or sets the design status of the Flange Steel Rib
-------------------------------------
Getter Method
Signature
DesignStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DesignStatus(designStatus)
Parameters: designStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
DisplayStatus¶
-
FlangeSteelRibChildBuilder.
DisplayStatus
¶ Returns or sets the display status of the Flange Steel Rib
-------------------------------------
Getter Method
Signature
DisplayStatus()
Returns: Return type: bool New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
DisplayStatus(displayStatus)
Parameters: displayStatus (bool) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Offset¶
-
FlangeSteelRibChildBuilder.
Offset
¶ Returns or sets the offset of the Flange Steel Rib
-------------------------------------
Getter Method
Signature
Offset()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Offset(offset)
Parameters: offset (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Plane¶
-
FlangeSteelRibChildBuilder.
Plane
¶ Returns or sets the plane of the Flange Steel Rib
-------------------------------------
Getter Method
Signature
Plane()
Returns: Return type: NXOpen.ISurface
New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Plane(plane)
Parameters: plane ( NXOpen.ISurface
) –New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
SheetMetalDistance¶
-
FlangeSteelRibChildBuilder.
SheetMetalDistance
¶ Returns or sets the sheet metal distance of the Flange Steel Rib
-------------------------------------
Getter Method
Signature
SheetMetalDistance()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
SheetMetalDistance(sheetMetalDistance)
Parameters: sheetMetalDistance (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Thickness¶
-
FlangeSteelRibChildBuilder.
Thickness
¶ Returns or sets the thickness of the Flange Steel Rib
-------------------------------------
Getter Method
Signature
Thickness()
Returns: Return type: float New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
Thickness(thickness)
Parameters: thickness (float) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
UseAngle¶
-
FlangeSteelRibChildBuilder.
UseAngle
¶ Returns or sets the use angle toggle of the Flange Steel Ribs
-------------------------------------
Getter Method
Signature
UseAngle()
Returns: Return type: int New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
-------------------------------------
Setter Method
Signature
UseAngle(useAngle)
Parameters: useAngle (int) – New in version NX4.0.0.
License requirements: ug_die_design (“Die Design”)
Method Detail¶
Validate¶
-
FlangeSteelRibChildBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.