FillAreaBuilderUpperLimitTypes Enumeration

NXOpen.Die.FillAreaBuilder.UpperLimitTypes is an alias for NXOpen.Die.FillAreaBuilderUpperLimitTypes

class NXOpen.Die.FillAreaBuilderUpperLimitTypes

Bases: object

Specifies how the upper limit of the fill area is defined.

Enum Members

Enum Member Enum Member Description
Sheet
Upper limit is defined by a sheet body.
Plane
Upper limit is defined by a plane.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.