FillAreaBuilderTypes Enumeration

NXOpen.Die.FillAreaBuilder.Types is an alias for NXOpen.Die.FillAreaBuilderTypes

class NXOpen.Die.FillAreaBuilderTypes

Bases: object

Identifies the area of the casting the fill is targeted for.

Enum Members

Enum Member Enum Member Description
BaseFlange
Fill area is in the base flange area.
ProductContact
Fill area is in the upper deck where relief for the product has been added.
ScrapArea
Remove the volume instead of filling. Targeted for the outer trim line area.
UserDefined
The user must defined all the constraints for the area (inputs from the target are ignored).
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.