DrawBeadSegmentBuilderMaleBeadWidthTypes Enumeration

NXOpen.Die.DrawBeadSegmentBuilder.MaleBeadWidthTypes is an alias for NXOpen.Die.DrawBeadSegmentBuilderMaleBeadWidthTypes

class NXOpen.Die.DrawBeadSegmentBuilderMaleBeadWidthTypes

Bases: object

value for how the male width is specified.

Enum Members

Enum Member Enum Member Description
Constant
The male bead width is specified by a constant value.
Derived
The male bead width is derived from the width specified for the female.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.