DrawBeadBuilderTransitionDefinitionTypes Enumeration¶
NXOpen.Die.DrawBeadBuilder.TransitionDefinitionTypes is an alias for NXOpen.Die.DrawBeadBuilderTransitionDefinitionTypes
-
class
NXOpen.Die.
DrawBeadBuilderTransitionDefinitionTypes
¶ Bases:
object
Specifies how the transition area should be determined from segment to segment within a single bead.
Enum Members
Enum Member Enum Member Description Automatic Shorten the bead segment that has the lowest height.Manual User specified start and end segments so transition areas are fully defined.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-