DrawBeadBuilderOrientationTypes Enumeration¶
NXOpen.Die.DrawBeadBuilder.OrientationTypes is an alias for NXOpen.Die.DrawBeadBuilderOrientationTypes
-
class
NXOpen.Die.
DrawBeadBuilderOrientationTypes
¶ Bases:
object
Identifies the orientation of the base parameters to the sheet metal.
Enum Members
Enum Member Enum Member Description Orthogonal The width and angle parameters are orthogonal, or normal, to the sheet metal normal at the section location.Vertical The width and angle parameters are oriented along the draw direction at the section location.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-