DrawBeadBuilderFemaleDepthTypes Enumeration

NXOpen.Die.DrawBeadBuilder.FemaleDepthTypes is an alias for NXOpen.Die.DrawBeadBuilderFemaleDepthTypes

class NXOpen.Die.DrawBeadBuilderFemaleDepthTypes

Bases: object

Specifies how the female depth is calculated or defined.

Enum Members

Enum Member Enum Member Description
Derived
The female depth is derived from the male bead (Max Male Depth + Constant).
Constant
The female depth is a user specified constant.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.