DiePlaneBuilderPlaneType Enumeration¶
NXOpen.Die.DiePlaneBuilder.PlaneType is an alias for NXOpen.Die.DiePlaneBuilderPlaneType
-
class
NXOpen.Die.
DiePlaneBuilderPlaneType
¶ Bases:
object
the options available for defining the plane
Enum Members
Enum Member Enum Member Description Selection Select the plane to be used.Plane Define the plane to be used.CoordinateSystem Define a coordinate system to specify the plane.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-