DieLocationBuilderLocationType Enumeration

NXOpen.Die.DieLocationBuilder.LocationType is an alias for NXOpen.Die.DieLocationBuilderLocationType

class NXOpen.Die.DieLocationBuilderLocationType

Bases: object

the options available for defining the location

Enum Members

Enum Member Enum Member Description
SelectLocation
Select the point to be used.
NewPoint
Define the point to be used.
NewCoordinateSystem
Define a coordinate system to specify the location.
NewVector
Define a vector to specify the location.
NewPlane
Define a plane to specify the location.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.