DieDirectionBuilderDirectionType Enumeration

NXOpen.Die.DieDirectionBuilder.DirectionType is an alias for NXOpen.Die.DieDirectionBuilderDirectionType

class NXOpen.Die.DieDirectionBuilderDirectionType

Bases: object

the options available for defining the direction

Enum Members

Enum Member Enum Member Description
Selection
Select a coordinate system (-Z) or plane for the direction.
CoordinateSystem
Define a coordinate system (-Z) for the direction.
Vector
Define a vector for the direction.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.