DieBooleanBuilderBooleanType Enumeration

NXOpen.Die.DieBooleanBuilder.BooleanType is an alias for NXOpen.Die.DieBooleanBuilderBooleanType

class NXOpen.Die.DieBooleanBuilderBooleanType

Bases: object

boolean type to apply to the selected solids

Enum Members

Enum Member Enum Member Description
Unite
Unite the solids to the application solid.
Subtract
Subtract the solids from the application solid.
Intersect
Intersect the solids with the application solid.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.