CompensateRoughDataBuilderTypes Enumeration

NXOpen.Die.CompensateRoughDataBuilder.Types is an alias for NXOpen.Die.CompensateRoughDataBuilderTypes

class NXOpen.Die.CompensateRoughDataBuilderTypes

Bases: object

Settings for the type of data being compensated.

Enum Members

Enum Member Enum Member Description
SheetBody
Sheet bodies being compensated.
Curve
Curves being compensated.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.