CompensateRoughDataBuilderApproximationType Enumeration

NXOpen.Die.CompensateRoughDataBuilder.ApproximationType is an alias for NXOpen.Die.CompensateRoughDataBuilderApproximationType

class NXOpen.Die.CompensateRoughDataBuilderApproximationType

Bases: object

Settings for the amount of approximation to perform.

Enum Members

Enum Member Enum Member Description
Coarse
Perform a coarse approximation.
Rough
Perform a rough approximation.
Fine
Perform a fine approximation.
Exact
Perform no approximation.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.