ClearanceBuilderTypes Enumeration

NXOpen.Die.ClearanceBuilder.Types is an alias for NXOpen.Die.ClearanceBuilderTypes

class NXOpen.Die.ClearanceBuilderTypes

Bases: object

Identifies which clearance type is being created in the casting.

Enum Members

Enum Member Enum Member Description
Gage
Clearance will be provided encompassing gage solids.
Gripper
Clearance will be provided encompassing gripper, or transfer, machinery solids.
Lifter
Clearance will be provided encompassing interior casting lifting solids.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.