ClearanceBuilderClearanceGeometryTypes Enumeration

NXOpen.Die.ClearanceBuilder.ClearanceGeometryTypes is an alias for NXOpen.Die.ClearanceBuilderClearanceGeometryTypes

class NXOpen.Die.ClearanceBuilderClearanceGeometryTypes

Bases: object

Identifies which type of input defines the clearance.

Enum Members

Enum Member Enum Member Description
Solid
The input is solids.
Section
The input is closed profiles.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.