AddendumSectionBuilderSegmentType Enumeration

NXOpen.Die.AddendumSectionBuilder.SegmentType is an alias for NXOpen.Die.AddendumSectionBuilderSegmentType

class NXOpen.Die.AddendumSectionBuilderSegmentType

Bases: object

The settings to indicate the segment type to update.

Enum Members

Enum Member Enum Member Description
Plus
Update plus segment.
Punch
Update punch segment.
FirstStretchWall
Update first stretch wall segment.
Reverse
Update reverse segment.
TrimLedge
Update trim ledge segment.
DiePunch
Update die punch segment.
SecondStretchWall
Update second stretch wall segment.
DieReverse
Update die reverse segment.
FlatToBead
Update flat to bead segment.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.