AddendumSectionBuilderSegmentParameterType Enumeration¶
NXOpen.Die.AddendumSectionBuilder.SegmentParameterType is an alias for NXOpen.Die.AddendumSectionBuilderSegmentParameterType
-
class
NXOpen.Die.
AddendumSectionBuilderSegmentParameterType
¶ Bases:
object
The settings to indicate which parameter of the segment to lock.
Enum Members
Enum Member Enum Member Description Length The length parameter of a straight segment.Angle The angle parameter of a straight segment.Radius The radius parameter of an arc segment.ArcLength The arc length parameter of an arc segment.-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-