AddSurfBuilderMethods Enumeration

NXOpen.Die.AddSurfBuilder.Methods is an alias for NXOpen.Die.AddSurfBuilderMethods

class NXOpen.Die.AddSurfBuilderMethods

Bases: object

Settings for the type of addendum surface being created.

Enum Members

Enum Member Enum Member Description
Sectional
Sweep section around tangency curve.
CurveMesh
Modeling curve mesh.
ChannelTunnelCap
To close an end cap.
MultiFaceBlend
Face blend between sets of walls.
WallsOnly
Produces just the walls, no blend.
DiskFaceBlend
Disk type face blend.
SphereFaceBlend
Spherical type face blend.
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.