SheetBordersAndZonesCollection Class¶
-
class
NXOpen.Diagramming.
SheetBordersAndZonesCollection
¶ Bases:
object
Represents a collection of
NXOpen.Diagramming.SheetBordersAndZones
objectsTo obtain an instance of this class, refer to
NXOpen.Diagramming.DiagrammingManager
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateSheetBordersAndZonesBuilder | Creates a borders and zones builder @return SheetBordersAndZonesBuilder object |
FindObject | Finds the NXOpen.Diagramming.SheetBordersAndZones with the given name. |
Method Detail¶
CreateSheetBordersAndZonesBuilder¶
-
SheetBordersAndZonesCollection.
CreateSheetBordersAndZonesBuilder
¶ Creates a borders and zones builder
Signature
CreateSheetBordersAndZonesBuilder(bordersAndZones)
Parameters: bordersAndZones ( NXOpen.Diagramming.SheetBordersAndZones
) –NXOpen.Diagramming.SheetBordersAndZones
to be redefined, if None then creates a new oneReturns: SheetBordersAndZonesBuilder object Return type: NXOpen.Diagramming.SheetBordersAndZonesBuilder
New in version NX10.0.0.
License requirements: drafting (“DRAFTING”)
FindObject¶
-
SheetBordersAndZonesCollection.
FindObject
¶ Finds the
NXOpen.Diagramming.SheetBordersAndZones
with the given name.An exception will be thrown if no object can be found with the given name.
Signature
FindObject(name)
Parameters: name (str) – Drawing sheet name Returns: Borders and zones object Return type: NXOpen.Diagramming.SheetBordersAndZones
New in version NX10.0.0.
License requirements: None.