NodeCollection Class¶
-
class
NXOpen.Diagramming.
NodeCollection
¶ Bases:
object
Represents a collection of Node.
To obtain an instance of this class, refer to
NXOpen.Diagramming.DiagrammingManager
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateNodeBuilder | Creates a NXOpen.Diagramming.NodeBuilder . |
FindObject | Finds the NXOpen.Diagramming.Node with the given identifier as recorded in a journal. |
Method Detail¶
CreateNodeBuilder¶
-
NodeCollection.
CreateNodeBuilder
¶ Creates a
NXOpen.Diagramming.NodeBuilder
.Signature
CreateNodeBuilder(node)
Parameters: node ( NXOpen.Diagramming.Node
) –NXOpen.Diagramming.Node
to be edited, if None then create a new oneReturns: Return type: NXOpen.Diagramming.NodeBuilder
New in version NX10.0.0.
License requirements: None.
FindObject¶
-
NodeCollection.
FindObject
¶ Finds the
NXOpen.Diagramming.Node
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with given name.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: NXOpen.Diagramming.Node
with this name.Return type: NXOpen.Diagramming.Node
New in version NX10.0.0.
License requirements: None.