DiagrammingAnnotationboundarytype Enumeration¶
-
class
NXOpen.Diagramming.
DiagrammingAnnotationboundarytype
¶ Bases:
object
Represents the boundary type of annotation.
New in version NX10.0.0.
Enum Members
Enum Member Enum Member Description NotSet No Boundary TypeCircle Circle TypeEllipse Ellipse TypeRectangle Rectangle TypeRoundedRectangle Rounded Rectangle Type-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-