ConnectionLocationBuilder Class¶
-
class
NXOpen.Diagramming.
ConnectionLocationBuilder
¶ Bases:
NXOpen.Diagramming.LocationBuilder
Represents a ConnectionLocationBuilder.
This is a sub-builder class and cannot be directly instantiated
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
EvaluatedValueX | Returns the evaluated X coordinate value that is the result calculated by the input percentage and offset. |
EvaluatedValueY | Returns the evaluated Y coordinate value that is the result calculated by input percentage and offset. |
InputPercentX | Returns or sets the user input percentage (0. |
InputPercentY | Returns or sets the user input percentage (0. |
InputValueX | Returns or sets the user input X coordinate. |
InputValueY | Returns or sets the user input Y coordinate. |
Reference | Returns or sets the sheet element whose coordinate system the coordinate is specified in. |
SegmentIdentifier | Returns or sets the segment identifier. |
Tag | Returns the Tag for this object. |
UpToDate | Returns the up to date flag. |
Methods¶
Method | Description |
---|---|
SetValueX | Set the x value of the location. |
SetValueY | Set the y value of the location. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
SegmentIdentifier¶
-
ConnectionLocationBuilder.
SegmentIdentifier
¶ Returns or sets the segment identifier.
-------------------------------------
Getter Method
Signature
SegmentIdentifier()
Returns: Return type: int New in version NX10.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
SegmentIdentifier(segmentId)
Parameters: segmentId (int) – New in version NX10.0.0.
License requirements: None.
Method Detail¶
Validate¶
-
ConnectionLocationBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.