ConnectionCollection Class¶
-
class
NXOpen.Diagramming.
ConnectionCollection
¶ Bases:
object
Represents a collection of connection.
To obtain an instance of this class, refer to
NXOpen.Diagramming.DiagrammingManager
New in version NX10.0.0.
Methods¶
Method | Description |
---|---|
CreateConnectionBuilder | Creates a NXOpen.Diagramming.ConnectionBuilder . |
FindObject | Finds the NXOpen.Diagramming.Connection with the given identifier as recorded in a journal. |
Method Detail¶
CreateConnectionBuilder¶
-
ConnectionCollection.
CreateConnectionBuilder
¶ Creates a
NXOpen.Diagramming.ConnectionBuilder
.Signature
CreateConnectionBuilder(connection)
Parameters: connection ( NXOpen.Diagramming.Connection
) –NXOpen.Diagramming.Connection
to be edited, if None then create a new oneReturns: Return type: NXOpen.Diagramming.ConnectionBuilder
New in version NX10.0.0.
License requirements: None.
FindObject¶
-
ConnectionCollection.
FindObject
¶ Finds the
NXOpen.Diagramming.Connection
with the given identifier as recorded in a journal.An exception will be thrown if no object can be found with given name.
Signature
FindObject(journalIdentifier)
Parameters: journalIdentifier (str) – Identifier to be found Returns: NXOpen.Diagramming.Connection
with this name.Return type: NXOpen.Diagramming.Connection
New in version NX10.0.0.
License requirements: None.