BulkEditBuilder Class¶
-
class
NXOpen.Diagramming.
BulkEditBuilder
¶ Bases:
NXOpen.Builder
Represents a BulkEditBuilder to edit bulk of objects.
To create a new instance of this class, use
NXOpen.Diagramming.DiagrammingManager.CreateBulkEditBuilder()
New in version NX10.0.0.
Properties¶
Property | Description |
---|---|
RenderingProperties | Returns the line rendering properties. |
Tag | Returns the Tag for this object. |
Methods¶
Method | Description |
---|---|
Commit | Commits any edits that have been applied to the builder. |
Destroy | Deletes the builder, and cleans up any objects created by the builder. |
GetCommittedObjects | For builders that create more than one object, this method returns the objects that are created by commit. |
GetObject | Returns the object currently being edited by this builder. |
SetDeltaXCoordinate | Sets the delta value of X coordinate for bulk moving. |
SetDeltaYCoordinate | Sets the delta value of Y coordinate for bulk moving. |
SetHide | Sets the visibility of sheet elements. |
SetHideLabel | Sets the visibility of labels. |
SetSheetElements | Sets the sheet elements for bulk editing. |
ShowResults | Updates the model to reflect the result of an edit to the model for all builders that support showing results. |
Validate | Validate whether the inputs to the component are sufficient for commit to be called. |
Property Detail¶
RenderingProperties¶
-
BulkEditBuilder.
RenderingProperties
¶ Returns the line rendering properties.
-------------------------------------
Getter Method
Signature
RenderingProperties()
Returns: Return type: NXOpen.Diagramming.RenderingPropertiesBuilder
New in version NX10.0.0.
License requirements: None.
Method Detail¶
SetDeltaXCoordinate¶
-
BulkEditBuilder.
SetDeltaXCoordinate
¶ Sets the delta value of X coordinate for bulk moving.
Signature
SetDeltaXCoordinate(deltaXCoordinate)
Parameters: deltaXCoordinate (float) – New in version NX10.0.0.
License requirements: None.
SetDeltaYCoordinate¶
-
BulkEditBuilder.
SetDeltaYCoordinate
¶ Sets the delta value of Y coordinate for bulk moving.
Signature
SetDeltaYCoordinate(deltaYCoordinate)
Parameters: deltaYCoordinate (float) – New in version NX10.0.0.
License requirements: None.
SetHide¶
-
BulkEditBuilder.
SetHide
¶ Sets the visibility of sheet elements.
Signature
SetHide(hide)
Parameters: hide (bool) – New in version NX11.0.0.
License requirements: None.
SetHideLabel¶
-
BulkEditBuilder.
SetHideLabel
¶ Sets the visibility of labels.
Signature
SetHideLabel(hideLabel)
Parameters: hideLabel (bool) – New in version NX11.0.0.
License requirements: None.
SetSheetElements¶
-
BulkEditBuilder.
SetSheetElements
¶ Sets the sheet elements for bulk editing.
Signature
SetSheetElements(sheetElements)
Parameters: sheetElements (list of NXOpen.Diagramming.SheetElement
) –New in version NX10.0.0.
License requirements: None.
Validate¶
-
BulkEditBuilder.
Validate
¶ Validate whether the inputs to the component are sufficient for commit to be called.
If the component is not in a state to commit then an exception is thrown. For example, if the component requires you to set some property, this method will throw an exception if you haven’t set it. This method throws a not-yet-implemented NXException for some components.
Signature
Validate()
Returns: Was self validation successful Return type: bool New in version NX3.0.1.
License requirements: None.