AnnotationBuilderTextTypeOption Enumeration¶
NXOpen.Diagramming.AnnotationBuilder.TextTypeOption is an alias for NXOpen.Diagramming.AnnotationBuilderTextTypeOption
-
class
NXOpen.Diagramming.
AnnotationBuilderTextTypeOption
¶ Bases:
object
Represents the option
NXOpen.Diagramming.AnnotationBuilder.TextType()
for aNXOpen.Diagramming.AnnotationBuilder
.New in version NX10.0.0.
Enum Members
Enum Member Enum Member Description Fixed Setting the text type fixedParametric Setting the text type parametric-
ValueOf
()¶ Returns enum member equivalent to the value passed. Useful for bit operations of enum members.
Signature
ValueOf(value)
Parameters: value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed. Return type: Enum Member type. New in version NX9.0.1.
License requirements: None.
-