WireGuide Class¶
-
class
NXOpen.CAM.
WireGuide
¶ Bases:
NXOpen.TaggedObject
Represents a wire guide object
To create a new instance of this class, use
NXOpen.CAM.WireTool.CreateWireGuide()
New in version NX9.0.0.
Properties¶
Property | Description |
---|---|
CornerRadius | Returns or sets the corner radius |
Diameter | Returns or sets the diameter |
Length | Returns or sets the length |
Tag | Returns the Tag for this object. |
TaperAngle | Returns or sets the taper angle |
Methods¶
Property Detail¶
CornerRadius¶
-
WireGuide.
CornerRadius
¶ Returns or sets the corner radius
-------------------------------------
Getter Method
Signature
CornerRadius()
Returns: the corner radius Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
CornerRadius(radius)
Parameters: radius (float) – the corner radius New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
Diameter¶
-
WireGuide.
Diameter
¶ Returns or sets the diameter
-------------------------------------
Getter Method
Signature
Diameter()
Returns: the diameter Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Diameter(diameter)
Parameters: diameter (float) – the diameter New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
Length¶
-
WireGuide.
Length
¶ Returns or sets the length
-------------------------------------
Getter Method
Signature
Length()
Returns: the length Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
Length(length)
Parameters: length (float) – the length New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)
TaperAngle¶
-
WireGuide.
TaperAngle
¶ Returns or sets the taper angle
-------------------------------------
Getter Method
Signature
TaperAngle()
Returns: the taper angle Return type: float New in version NX9.0.0.
License requirements: None.
-------------------------------------
Setter Method
Signature
TaperAngle(angle)
Parameters: angle (float) – the taper angle New in version NX9.0.0.
License requirements: cam_base (“CAM BASE”)