WedmGeomBuilderBackburnPassesTypes Enumeration

NXOpen.CAM.WedmGeomBuilder.BackburnPassesTypes is an alias for NXOpen.CAM.WedmGeomBuilderBackburnPassesTypes

class NXOpen.CAM.WedmGeomBuilderBackburnPassesTypes

Bases: object

the types available for wedm backburn passes

New in version NX7.5.0.

Enum Members

Enum Member Enum Member Description
Single
single backburn pass
MultipleRegionFirst
multiple backburn passes - region first
MultipleCutoffFirst
multiple backburn passes - cutoff first
ValueOf()

Returns enum member equivalent to the value passed. Useful for bit operations of enum members.

Signature ValueOf(value)

Parameters:value – Any integer value or bit operation result of enum members:type value: int:returns: Enum member equivalent to the value passed.
Return type:Enum Member type.

New in version NX9.0.1.

License requirements: None.